Part Number: OPA857EVM
Other Parts Discussed in Thread: OPA857
Hi Samir,
I hope you're doing great. I just purchased the EVM for OPA857, and I am still operating in test mode.
The test results, however, do not conform to the specifications: I am setting the input DC bias as specified in the manual (Find VIN1 = OUT = OUTN = 1.83, then VIN2 to have OUT = 1.33, and make VIN DC = (VIN1 + VIN2)/2. I end up with DC ~ 2.08V, and AC ~ 240 mV.
However, when I apply this input, and an AC of VIN1-VIN2, I do not get the gain specified.
In fact, when I probe OUT and OUTN, I got only a considerable signal from OUT, and a very low signal from OUTN. Also, the signals are not differential, and the output swing is around 70 mV for an input voltage of 240 mV. The output signal from OUT maxes out ~ 150mVp-p, and the signal of OUTN maxes out @ few mV. Any thoughts?
My understanding is that the signals will be differential (at the output of the TIA when I probe them). I also expect the output swing to be ~500 mV for 3.3V supply.
Best,
Gerard