This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC6001: Why -IN is short-circuit with GND? How I broken it?

Part Number: LMC6001
Other Parts Discussed in Thread: LM358, LMC6081

I am designing a signal amplification circuit using LMC6001BIN.

the schematic is like this:

Before I test this current I test my LMC6001, It is ok. And I also check my circuit map and it is just like this schematic.When I power it on, I find the temperature is so high. And it is not work as what I want. So I test it and I find Pin2(-IN) is short-current with Pin4(GND). And I get signal voltage is about 8.5V .And I remove this chip and test it. And yes it is broken.

(Ip[current] on D1 is 0.7uA at most by the way.)

But I don't know why but I am sure I am wrong. So help me, Thanks? If the amplification ratio what I design is too high.

(I am a chinese so my english is not so good, I translate it to Chinese. Thanks)

我使用上面的电路去做一个光电二极管的放大电路。因为我的输入电流至多0.7uA,所以我设计这个电路端的电压等于Ip*R3*(1+R2/R1)

但是在我上电之后(尚没有给予光线照射),发现输出信号一直是8.5V左右,然后我察觉到芯片温度很高,所以我断电取下芯片测试发现LMC6001的pin2和pin4短路。

我个人觉得一定是我使用这个芯片没有注意哪些参数导致的。是不是我的放大倍数太大了?

而且我检查了电路确认电路和原理图是一致的。

请您给与帮助,谢谢。

  • Part Number: LMC6001

    I am design a signal amplifier circuit. But I don't know why my LMC6001 is broken. And here is the basic schamatic.

    I am afriad if I give a such large amplification.  Cause my signal Ip is really small, it is 0.6uA max. (Ip is the current of D1 and D1 is a photodiode)

     When I powen on my circuit just for a while. I find LMC6001 is really hot, and I don't get a right output. When I power off and take LMC6001 off and test it. I find Pin2(-IN) and Pin4(GND) is short-circuit.

    Please help me. Thanks.

    By the why, the chip is LMC6001BIN。

  • John,

    First and most important is to faithfully follow safe ESD prevention procedures.
    Be sure that 12V supply doesn't spike above 15.5V during power up/down/running.
    Is this a new or old design? Measure ICC on a new device; is ICC high right from the start or does it increase later?
    0.7uA * 1Mohm * 21 = 14.7V , so yes the gain is too high. However that will not break the LMC6001.
  • Ron,

     Thanks very much. You are right about the very high gain.

     And this design  refer to the design in 《Photodioda amplifiers op amp solutions》,Jerald Graeme.

    And I use multisim to simulation this design, It is work well. 

    And I have modified my design. Change  R2  from 20K to 10K. And change R3 from 1M to 500k.(Actually, I have two different sense. another have a small If. So I design like this). It seem like ths didn't solve this problem.

    Yes, I am sure ESD is important. And I build this circuit by hand and I want to test it first and then design PCB file. Maybe I didn't check every net-connect on my circuit.

    I will let you now If I solve it.

    Thanks

  • Ron:

          I think I need tell U my solution.

          When I check my LMC6001, I find mark on this chip is NS not TI. So maybe this is an old product or fake one. Cause I haven't a new one  at hand. So I use LM358 to test this circuit. And It worked well. 

    And I have order some new LMC6001 and LMC6081. And I will test again.

          Have a good time. Thanks again.

  • The NS symbol is still used on this device.