This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm struggling to wrap my head around which ADC to use for the digitization of the photodiode signal that comes from the LOG114. I presume that I'll need a very high resolution ADC to get resolution across the entire 8 decades of amplifier range, but I'm not sure which architecture and resolution to choose. The implementation is used to measure scattered light from smooth surfaces and spectral reflectance of relatively high intensity - thus the need for 8 decades of range. Please provide a suggestion and a EVM that I could attach to the LOG114 EVM would be great.
Thank you,
Patrick