This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LOG114: Can I use one of the available OP Amps on the LOG114 as a buffer amp for Vref on the ADC?

Part Number: LOG114
Other Parts Discussed in Thread: ADS8866

Hello,

I'd like to use the daisy chain feature of the ADS8866, but I understand that using the same reference supply for an external ADC can be problematic if connected directly. Can I use one of the two available OP Amps on the LOG114 as a buffer amp for the ADC? So, the configuration is one LOG114 tied to one ADS8866 with Vref buffered thru LOG114 to provide Vref for ADS8866. I need to do this with three acquisition channels - one per photodetector.

Thank you,

Patrick