Part Number: XTR117
Other Parts Discussed in Thread: XTR111, XTR300
Hi there,
I'm looking to drive two process loops from a microcontroller, using a DAC7612U to generate the voltage and then feeding a pair of XTR117's to convert to 4-20mA. All power is supplied locally; in fact we actually need to supply 24V loop power from this device.
This is obviously very different to the application circuits of the XTR117; which all take loop power and supply the control circuitry.
Do you have a recommended circuit for this? In the 'XTR117 and Arduino PWM analog interfacing' thread you employ a considerable amount of filtering and isolation on the control side of the XTR117. Is this as necessary if we're supplying the loop power? I use a low-ripple DC-DC converter with primary side L-C filter to supply 5V to the microcontroller and 2ch DAC.
Any help you can offer would be much appreciated.