Part Number: OPA330
I am having a little difficulty understanding the impedance specifications. The data sheet for the OPA330 does not list any impedance values.
I did read a post in E2E that explained that you could calculate the common-mode impedance of an op amp (OPA330) by taking the change in the common mode voltage and dividing it by the change in the in the bias current. Many data sheets have a graph of this so calculating this is possible. I have done this calculation and it appears that the common-mode impedance of the OPA330 is (5V/5pA=) 1000Gohms. Is this the correct approach?
The issue that I am having is that the customer is asking for the differential impedance. This is not listed, but is there a way to calculate this? I did see a post that stated that if the op amp was produced using a CMOS process that you could estimate that the differential impedance would be 100Mohms and the common-mode impedance would be 6000Gohms. I am not sure if this applies to these chopper driven op amps like the OPA330. Can you elaborate at all on this? Are there any calculations available? Are there any impedance specifications available?
Thanks for your help with this!
Richard Elmquist