Part Number: OPA2197
一、Customer's FTU products,Acquisition of zero sequence voltage by electronic transformer,Load impedance requirement is greater than 5M:
二、Customers's’current circuit ,for system test,the input of AI15 = 6.5*1.2*1.414V,and the output AC0 ≈11.0V。More than the input of ADS8688S。
三、Please help to assess whether the following corrective measures are correct:
1、The output of the electronic transformer is divided by two 2.5M resistors in series and then input the ADC8688S.
2、The output of the VAC0 is divided by two 2.5M resistors in series and then input the ADC8688S.
3、If the signal is reduced directly by the amp(FU13A), it will affect the input impedance of the amplifier or not.(Demand is greater than 5M).
Thanks for kindly help.