This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Noise bellow 0.5V with OPA380

Other Parts Discussed in Thread: OPA380

Hello you all!

The schematic bellow shows the transimpedance amplifier which I have been using. The OPA380 is the operational amplifier in this case. I can not understand the reason that bellow 0.5V a 56KHz oscillation shows up and it disappears when the signal reaches almost 0V. Would it help to solve the problem if I use a supply voltage of -5 and 5V instead of GND and 5V? What could be the reason of this oscillation? I have checked if there could be some external influence but that doesn't seem to be the case.

Thanks for the attention!