This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE032: evm availability

Part Number: AFE032


Hello sirs,

i’ve read on the TI website that additional information can be requested on the availability of an evm for the AFE032 plc front-end.

Could you please send me some information on the availability of this evm:

- how it’s composed (AFE032 only or complete solution with the dsp processing chain);

- availability of AN/white papers/sample code or libraries for the processing path (modulation algos, …).

 

I’m still in a very early evaluation phase, and for this I cannot specify information such as quantities; the application would be to communicate data (at very low rate) over a 3-phase motor cable (probably without the neutral connection), fed by a CSI inverter (and this is the problem, because the CSI inverter has big phase-to-phase capacitors).

 

Thank you in advance for Your time.

Best regards