Other Parts Discussed in Thread: XTR111,
I have been using XTR111 IC's on two products we manufacture, one product has one XTR111 the other has two XTR111 both are controlled by a MCU that has analog outputs. We are having many problems with between the power supply for the MCU and the power used to drive the 4-20mA loops, which comes from a PLC or DCS. Without isolation I am having to pull a ground wire from the 4-20 input module to my 4-20 transmitter. Because of this I want to isolate the MCU power from the power from the 4-20mA module(s) on the controller. If I can do this I will expand the number of IC's to 6 per board.
I see three choices, have one isolated I2C bus powered by one of multiple XTR116 IC's, use multiple I2C isolators with each isolator powered by the Vreg and the DAC powered by the Vref of each XTR116, or bring isolated power from the MCU for the I2C and power each DAC with the Vreg of each XTR116.
I would prefer the first option:
Is the above workable? If not what are the alternatives.