Part Number: LM2903
Dears:
For LM2903.
Supply voltage: 5V
Input voltage:0-36V
What gonna happen?
Could it work correctly?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2903
Dears:
For LM2903.
Supply voltage: 5V
Input voltage:0-36V
What gonna happen?
Could it work correctly?
Thanks
Hello Zhengqing,
For the LM2903 family, it *might* work depending on the input conditions.
The inputs can be taken up to 36V regardless of supply voltage without damage - but that does not mean the output will be correct..
The output will be correct *if* one of the inputs is within the valid input range (0 to 3V on a 5V supply).
See section 8.2.2.1 in the Applications section and table note 2 on page 7 for more information.