Hi,
I built the following circuit to measure the noise floor of OPA388. R2=200k ohm, R1=100 ohm (precision metal resistors). The op amp is power by + - 3 V lithium batteries. I then recorded the output using 24-bit NI DAQ board with a sampling rate of 1 kHz. I calculated PSD using Matlab periodogram function, and finally divided sqrt (PSD) by the gain (1+R2/1R1=2001), referring the noise back to the input.
The resulting noise PSD (V/sqrt Hz) is shown below. I also included the noise plot from OPA388 data sheet for a comparison. Above 1 Hz, the noise is 3-4 times larger than the value reported in the data sheet (7 nV/sqrt Hz). What concerns me more is the 1/f region. OPA 388 should have zero 1/f noise according to the data sheet. Does anybody know why? I also measured the noise floor of NI DAQ board by short circuiting its input. It is much smaller, especially at low frequency region. So I know it is not caused by DAQ.