Part Number: OPA2376
Hi,
Let me confirm about below.
* According to datasheet, there is following description.
"The OPAx376 in a unity-gain configuration can directly drive up to 250pF of pure capacitive load."
Is there any restriction of input/output signal in above condition ?
Especailly, what I would like you to confirm are
1. Is there any restriction for "output current" ?
2. Is there any restriction for "frequency of input signal" ?
Best regards,
Machida