Part Number: LMV7235
Team,
My customer has the following comment and needs clarification.
LMV7235 data sheet section 8.3.1 states that "If one of the inputs goes above the positive common mode limit, the output will still maintain the correct logic level as long as the other input stays within the common mode range". Testing has revealed this to be true only if the input current to the pin is below approximately 0.35mA (room temp). If the pin current exceeds this threshold, the output flips to the wrong state. There is a /-10mA abs max input current constraint but, if confirmed, this additional functional constraint should be provided in the datasheet.
Regards,
Aaron