Part Number: LMH7324
Hi All,
Need one clarification on the part LMH7324SQ.
Can you please advise what will be the expected output voltage levels for VCCO=1.8v , will it be VOH=0.7v & VOL=0.3v?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMH7324
Hi All,
Need one clarification on the part LMH7324SQ.
Can you please advise what will be the expected output voltage levels for VCCO=1.8v , will it be VOH=0.7v & VOL=0.3v?
thanks
Hi Siddarth,
VOH and VOL will be relative to VCCO. The high level of the output is normally 1.1V below VCCO and the low level is normally 1.5V below VCCO. So in your case you are correct that VOH = 0.7V and VOL = 0.3V.
Regards,
Jaskaran
thanks for the reply. in my case VE=-5v, VCCI=4.5V & VCCO=1.8V , is that fine ? also can you please advise on the following :