This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA125: Load Cell Amplifier Circuit

Part Number: INA125


Hello - I'm hoping someone could help point us in the right direction on this issue. We are using the INA12UA as an amplifier for a load cell bridge measurement circuit with two different load cells. We've gotten the circuit to perform well with one load cell, but are having issues getting the expected output with the other type.

The amplifier is being powered with 5V, which is also the excitation voltage for the load cell bridge. In one configuration, we are using a 20mV/V load cell and use an Rg = 1K for a gain of approximately 64. This configuration seems to work well. However, using the 1mV/V load cell with an Rg=60.4, the output of the amplifier doesn't seem to change regardless of the load on the load cell which will generate a differential voltage between 500µV and 5mV. It hovers right around 60mV.

My guess is that the amplifier offset voltage drowns out any signal the 1mV/V load cell, and this 60mV is the gain being applied to the offset voltage, but we don't have enough experience with this type of circuit to be sure of that. If that's the case, is there anything we can do to read this 1mV/V load cell? Would a different amplifier be required? Would there be an amplifier that could handle signals in the range previously mentioned and still be able to drive an output in the 3.3V/5V range?

  • Hello ewilliamstextron,

    You mention, "However, using the 1mV/V load cell with an Rg=60.4, the output of the amplifier doesn't seem to change regardless of the load on the load cell which will generate a differential voltage between 500µV and 5mV. It hovers right around 60mV."

    Is 60 mV the voltage you mesure at the INA125, Pin 11, output with respect to ground? If so, that the would indicate that the A1 output (see datasheet Figure 6) is in saturation. Once the output is in saturation changing the input differential voltage will have almost no effect on the output voltage. If everything is set up and operating correctly you wouldn't expect the output to be in saturation.

    Your INA125 gain is set to about 1000x so any unexpected input offset in addtion to the natural offset of the INA125 would be multiplied by that very high gain. The total output referred offset could be large enough such that the output is driven to a level 60 mV above ground.

    If you can provide your INA125 schematic, information about your input load cell, and the output load we can look it over and see if we detect anything that is suspect.

    Regards, Thomas
    Precision Amplifiers Applications Engineering
  • Thomas,

    I wanted to thank you for taking the time and effort to analyze and respond. It turns out we were having a test setup issue, which once resolved, demonstrated the INA125 is performing as expected.

    Thanks again, Eric

  • Hi Eric,

    I am glad you were able to resolve the INA125 circuit issue on your own and that it is now working as expected.

    Good speed with your project!

    Regards, Thomas
    Precision Amplifiers Applications Engineering