This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: Cyclic voltammetry problem

Part Number: LMP91000

Hello,

I am working on a project where I make use of LMP91000 potentiostat for cyclic voltammetry (using amperometric mode). I have interfaced the LMP91000 with a PIC microcontroller and I am able to program it to vary the voltage between WE and RE from 0.8V (24% of my Vdd=3.3V) to -0.8 V. If I shortcircuit CE and RE to test the hardware (if doubt, please refer to Test 1 in page 23 of attached document en.DM00093722.pdf), I am able to vary Vwe-re between 0.8 and -0.8V.

However, when I place the sensor instead of shortcircuiting RE and CE, Vwe-re voltage is not capable of reaching the negative limit of -0.8 V. Instead, it stops at about -0.32 V. It does not matter how many cycles I try: it works well from 0.8 to -0.32 and back to 0.8V, but it is programmed to go down to -0.8V, which is never reached.

Please let me know if you can think of any possible causes of this problem or any solutions.

Thank you very much.

  • Hi Pablo,

    The Vout signal will depends on the type of sensor you use and the presence of the gas to detect. The presence of this gas will change the current going into the TIA (trans-impedance amplifier) and the Vout value will change accordingly. Not sure how you are trying to measure the dynamic range.
    What I recommend it In order to look at the LMP91000 Webench designer tool.
    This tool will generate the schematics and the register configuration for the LMP91000. You can also enter the parameters for your sensor of preference if the sensor / gas you are using is not there.

    Please click on the link below and Webench link will be in the right portion of the page.
    www.ti.com/.../lmp91000

    Regards,
    Jose