This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to use the INA240A2 in High-Side Current monitoring with electrical treatment to obtain the three motor phases equivalent current with one shunt/amplifier. (for cost and size reduction)
The sboa163a Fig3 application note describes this configuration.
In our design the power supply can vary from 15.5V to 46Vdc transient even 70V in lightning surge.
In our configuration, the measured current will be in discontinuous mode with high di/dt ( roughly 200A/µs, 20kHz switching frequency). Is the INA240 is adapted to this use or what other reference will be more compatible?
Thanks for your reply,
Regards
Hi Nicolas,
Thanks for choosing TI.
If I understand your requirement accurately, during normal operation the current sense amplifier will see a constant common mode voltage, and a differential input step of 20KHz; The actual profile of the differential step will be determined by the current profile and shunt impedance.
With these conditions in mind, INA240 should fit, however we have a number other potential candidates, including but not limited to INA193, INA200, INA282 and LMP8640 families. Aside from electrical specs, they differ in terms physical size and unit cost. I recommend review them based on parameters that are important to you.
Hope this helps, let us know if you have any more questions or if this resolved your issue.
Regard, Guang
Hi Guang
Thanks a lot for your fast reply.
The INA240 is given for 2V/µs slew rate but around 10µs settling time. It's too long compare to 50µs PWM period.
The INA193 is given for 1V/µs slew rate but around 2µs settling time. (faster than the previous one in some cases)
The INA301 whitch is seem to be suitable for my application is given for 4V/µs slew rate but no settling time given. This parameter can it be given?
My wish is to deform as little as possible the signal to be measured (0 to 4V output)
Thanks for your precious help,
Regards
Nicolas
Hi Nicolas,
Judging from Figure 24 of the data sheet, INA301 settling time is probably around 2uS as well. I agree INA301 will give faster large signal response compared with the other two.
Regard, Guang
Hi Nicolas,
I hope all is well and sorry for the late reply.
The bidirectional topology should work. The device functional mode descriptions still apply, as in section 8.4.2 in the datasheet. If low current level is a don’t-care, then it can be disregarded.
Common mode voltage in range (-16V, 80V) will not cause phase reversal. I think this is what your concern is.
A bit more on this topic however - some older amplifiers, when subjected to large differential input voltages, will exhibit this behavior. This device is one of them. The triggering level (many volts), nevertheless, is far away from the upper limit of the linear input range. Therefore during normal operations, the chance of phase reversal should be virtually 0. I think the only chance a phase reversal will ever happen is when the sense resistor vaporizes. And the full DC bus voltage appears across the input.
Since your input current is step waveform, it will be better to have low inductance sense resistors. If ringing is a potential problem, you may consider putting ferrite beads in the input sense lines. The optional input filters can aid in tamping down such ring as well.
Regard, Guang