This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using an OP547 in a non-inverting amplifier architecture. The amplifier has a bipolar +/- 15V supply. The gain is set to 5.22 (connected to a 2.5V reference). There is a 10K/100nF on the current limit pin (connected to -15V). I am using the D2PAK package.
When there is no load (infinite), the component heats up to ~ 55C.
What could cause this heat?
I read in another blog that the OP547 generates internal heat and needs a heat sink. If the PCB heat sink is too small (or any other problem), can the component heat up to 55C?
Thank you for your help
Pierre
Hello Pierre,
If the OPA547 DDPAK package is not soldered to a heatsink surface, then the thermal resistance from the op amp junctions to the air will be the θJA = 65°C/W listed in the datasheet Electrical Characteristics table. Since the semiconductor die internal to the OPA547 is attached directly to the metal DDPAK inner surface, it and the plastic material after several thermal time constants will eventually assume a temperature a little less than the actual Tj temperature.
Here are two scenarios based on the typical quiescent current of 10 mA, and the maximum quiescent current of 15 mA:
If Iq = 0.01 Amps typical, and (V+) - (V-) = 30 V
TJ = TA + θJA ∙ Pd
TJ = 25°C + 65°C/W [(30 V)(0.01A)]
TJ = 25°C + (65°C/W ∙ 0.3 W)
TJ = 44.5°C
If Iq = 0.015 Amps maximum, and (V+) - (V-) = 30 V
TJ = 25°C + 65°C/W [(30 V)(0.015A)]
TJ = 25°C + (65°C/W ∙ 0.45 W)
TJ = 54.3°C
You will note that in the second, maximum case the Tj ≈ 55°C. If the OPA547 is left powered "on" long enough the case will approach the same temperature. The OPA547 maximum specified Tj = 150°C; therefore, there isn't any issue with running the device with a Tj ≈ 55°C.
Note that the OPA547 DDPAK solder tab be electrically connected to the V- supply.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
Thank you very much for your detailed calculations.
Everything is explained now.
Pierre
Hello Pierre,
I am glad to be of assistance with your OPA547 inquiry.
Regards, Thomas
Precision Amplifiers Applications Engineerig