Part Number: LF353-N
Other Parts Discussed in Thread: LF347-N, LF347, LF353
Can you tell me the value of the input capacitance for the LF353-N?
Thanks for your help with this!
Richard Elmquist
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Richard,
I believe the capacitance will be the same as LF347-N (quad) two samples.
Cp is noninverting capacitance (to GND)
Cn is inverting capacitance (to GND)
Cd is input to input capacitance.
| LF347 | LF347 | |
| Cp | 3.3 pF | 3.4 pF |
| Cn | 3.5 pF | 3.7 pF |
| Cd | 1.4 pF | 1.9 pF |
I do not have data on LF353 (dual).