I have a beginner question, but somehow I have internal disagreement in that aspect.
I'm have design of system with diff op amp THS4521 that Gain is lower than 1
(Gain<1, Gain =Rf/Rg=Vout/Vin=0.1)
1. Please advice how can I test the stability of this circuit in spice simulator (i.e. Gain x Phase (in open loop?))?
1. If I'm know that the degree of an amplifier's stability can be quantified by a so-called stability factor
and the system will be stable at G1xG2 /= -1
In my case the G1< 1, so it means that system always are stable??? Please advice if I'm wrong.
I sow in some datasheet that written the "Amplifier is stable at Gain=1V/V". So what happen if Gain <1V/V ?
Thanks a lot for help. Roman.I.