This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE031: SPI Frame documentation error?

Part Number: AFE031
Other Parts Discussed in Thread: C2000WARE

In the AFE031 datasheet (SBOS531D), page 35, it states....

A host SPI frame consists of a R/W bit, a 6-bit register address, and eight data bits.

This lead me to believe the frame is 15 bits (where 6 bits are address).

But in C2000ware example

C:\ti\c2000\C2000Ware_1_00_03_00\device_support\f2837xd\examples\cpu1\boostxl_afe031_f28379d_pwmmode\cpu0\afe031_config.c

in function void HAL_afe031_regWrite(UINT16 addr, UINT16 data),

it appears the frame is 16 bits (1 RW bit, 7 address bits, 8 data bits).

 

Is the datasheet wrong or did I read it incorrectly?

 

Am I correct to think the SPI bits shift-out should be

RW | Addr6 |  Addr5 | Addr4 | Addr3 | Addr2 | Addr1 | Addr0 |  Data7 |  Data6 |  Data5 |  Data4 |  Data3 |  Data2 |  Data1 |  Data0

 

Thanks for your help.

  • Hi Quark,

    Sorry for the misleading sentence in the datasheet. From Tables 8 through 16 it is clear that there are actually a R/W bit and 7 address bits. I will pass this along for a correction in the next datasheet revision. If this resolves your current issue, please click the resolved button and open a new thread for further questions.

    Best regards,

    Sean

  • Thank you. Please also ask to rework Table 8. Instead of naming the Bit Names ADDR8 to ADDR14, it really should be ADDR0 to ADDR6 to represent the zero-th to sixth bits of the address.