This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying to figure out what the difference between these two devices is, aside from the temp range (LMV331 is specified up to 125°C) and price (LMV331 is 5 cents cheaper) I don't see any difference. Can you help clarify this?
Best regards,
Tadeo
Hello Gerardo,
The LMV331-N is the original National Semiconductor version, the LMV331 (non -N) is the TI second source.
After TI acquired National, all the "duplicate" National devices got a "-N suffix.
So they are similar..but slightly different as they are two different designs on two different processes by (at the time) two different companies, so there will be slight differences in the fringes of operation. But for the most part, other than the temperature range, they are the same.