Part Number: TLV2370
Tool/software: Linux
Dear Sirs,
We are using the TLV2370 in one of our boards and we have some doubts related with the shutdown pin of this part.
Actually, we do not pretend to make any use of the shutdown feature. So, we left the pin 8 of the ampop floating, as per datasheet instruction.
However, there is a strange behavior on the ampop. In some cases, the output goes to zero, without any reason for that. It seems that sometimes it is entering in shutdown mode.
In the datasheet, there are some considerations in the section "8.3.5 Shutdown Function" related with the leakage current in the shutdown pin. These statements are contradictory with the use of the shutdown pin in floating mode. Can you kindly clarify this question?
Best regards,
Oscar