This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6401: LMH6401 default gain setting

Part Number: LMH6401

Wondering if it is possible to get the LMH6401 with a different default value configured for the gain? Have an application where we desire it to always be set to max gain, not min.

  • Hello,

    Unfortunately the default of the LMH6401 gain register is set to the minimum gain. If you reset the device, it will always default to the minimum value. However, the power-down mode of the device retains the register values, so you can program the device initially and just use the power down function to reduce power consumption when you do not need it to be on.

    Regards,