Other Parts Discussed in Thread: INA139, INA169, INA138, INA168, INA240
Dear Sir,
Currently, i'm using INA139 with my charge controller for current sensing, which is 24V. Since the INA139 common mode voltage is around 36V. It is very useful for my application.Now I would like to design a 48V charge controller, also my battery voltage is maximum 60V. Can I able to use INA169-Q1 for my application. Common mode voltage for INA169 is 60V(operating condition) and 75V (absolute maximum rating).
- Power supply for the current sensor - 12V
- The allowable full-scale output voltage - 3.3V
- Device frequency response needed (do you want to measure AC or DC current?) - DC Current
- How low can common-mode voltage go? - 42V
Kindly please suggest whether I can use INA169 for my 43V-60V Battery Current sensor ?.