Part Number: INA117
Other Parts Discussed in Thread: INA828, INA188,
I'm attempting to repair a circuit for a large instrument. Based on how the circuit is situated, I am attempting to replace some of the op-amps in the circuit. My circuit contains the INA117BM High Common-Mode Voltage Difference Amplifier (TO-99-8 pin) and the INA114BP Precision Instrumentation Amplifier (DIP-8 pin). The issue I'm facing is that the amplifiers are old, and I can't find some of them on Digi-Key. The INA117BM is non-stocked, and it usually runs around $70. On the other hand, the INA114BP is available at the cost of around $13. Regardless of availability, I was wondering what suitable replacements would you recommend for the amplifiers, specifically the INA117BM?
Sorry, I forgot to mention this, but because I am repairing a new piece of equipment and not designing from scratch, I would prefer it if I can match the same layout style as the original amplifier. That would mean for replacing the INA117BM, I would prefer a TO-99-8 pin package or a DIP 8-pin package. It should be noted that the original INA117BM had its legs spread out such that it fit a DIP-8 pin socket, so I'm not necessarily looking to fit a TO-99 socket, but a DIP-8 socket.