Other Parts Discussed in Thread: ADS1255, OPA2333, OPA2350, OPA333, OPA350, OPA2365, OPA2727, ADS1256
Hi @all,
I'm using the ADS1255 with a radiometric interface. The Ref-Interface is like suggested: About 20uF between Ref+/-, driven by an OPA(2)350 as Unity-Gain-Amp.
So far the circuit is working well, Resolution/Noise is excellent!
But: A temperature-Scan is showing a Gain-Drift of about 1..2ppm, which is mainly due to the offset-drift of the Buffer-OP. (4uV/°C == 1.6ppm/°C @2.5V).
When changing the OP to a "zero-drift"-OP like the OPA2333, the Ref-Buffer-Circuit is instable and must be compensated. The drift now is like expected (<1ppm/°C), but I have to change my PCB (because of the compensation components).
So: Do you have a suggestion for a one-to-one replacement of the OPA2350?
Regards
Martin