This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR300: XTR300 Error Flags's pull-up resister.

Part Number: XTR300


Dear Sir,

XTR300  Error flags: EF_CM, EF_LD, EF_OT pull-up resister can put 1Kohm or 4.7Kohm ?

Please you kindly review & advise.

Thanks!

Steven

  • Steven
    The EF outputs can sink up to 5mA so you should be ok, however with a 5V supply and 1k you are right at the limit.
    Note: If you use the EFot output to drive the output disable pin you need to use 2.2k. See page 25 of the data sheet.


    If this answered your question please click the green "This Resolved My Issue" button