Hi all,
In the following circuit, when enable input is float, i see 700mV dc voltage at inverting input of opamp. Thus, there is 70uA current from inverting pin of the opamp. However, LM6172 datasheet states that max bias current is 4uA and max offset current is 3 uA. What is the reason of this current? Is this normal?
Best Regards,
Eren