Part Number: TL084
Other Parts Discussed in Thread: ADS1115, LM324, , TLV4170
Dear all,
I have a device that I measure its IV curve, this device's working voltage range is from -3 to 3 V, and in order to read the IV data I'm using the ADS1115, so I have to convert the device's input and output voltages to a unipolar signal from 0 to 3 V and to do this I'm using TL084CN , when I connect this opamp to the first terminal of the device the signal is converted successfully but when I do the same in the other terminal of the device where there is a resistor connected to measure the current, the negative side of the input signal of the opamp disappears and I see only the positive side, is that because of the common voltage range of the opamp? could someone explain this for me, the power supply of the opamp is -5 V and 5 V. The same thing happens when I connect LM324 opamp.
The circuit schematic is attached.
Thank you,