Other Parts Discussed in Thread: TLV171, TLV170
Hello there,
In my current design I am using MIC6211 as voltage buffer. The problem is (I noticed that later) its output voltage swing. The chip is powered from voltages varying from 12 V to 25 V (reference to ground). The voltage I need to buffer varies from 2V to 0V. Now its minimum swing is around 1.2 V and I need a maximum of 0.2 - 0.3 V. Are there any TI parts that would match the MIC6211 footprint and provide better swing? I would appreciate all help.