Part Number: LMH3401
Can I sum two 50 ohm input signals while maintaining isolation between the two sources? These opamps are currently in use on a prototype PCB and I need to maintain a 50 ohm input load impedance for each source. Currently the source impedance of one source degrades the input load impedance of the other source.