Part Number: INA199
Hi expert,
My customer has a question on INA199 sequence between V+ and input signal. They used INA199 to sense input current but the V+ is connected to 3.3VREF which is ready after input signal is present. But they don't want output out of control before V+ is present. I referred to below link for power sequence FAQ and found out if output connects 10kohm to GND then output would be kept at 0V(V+ is floating). They now connect 10kohm+15kohm as a voltage divider at output, as below picture.
Our question is whether Vout will be kept at 0V when V+ is not ready in their application(with this 25kohm). Could you kindly help on this case? Thanks!!
Best regards,
Ann Lien