This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA188: INA188-EP

Part Number: INA188
Other Parts Discussed in Thread: INA101, INA129, INA828

Hi,

Can you please provide the schedule when the extended temperature range version of the INA188 will be released?  Do you have a preliminary data sheet showing the specifications over the -55 to +125C temperature range?  Will the EP part be offered in the SOIC-8 and SON (DFN-8) packages?  Do you have the full part numbers of the INA188-EP parts?

Our application requires -55 to 125C operation.  Our power supplies are +/- 15V.  Do you have any other instrumentation or difference amplifiers in development that will have specification performance data over the -55 to 125C range that have similar performance to the INA188?  The gain error at G =1 needs to be less than or equal to 0.05% at 25C with a temperature drift error on the order of 5 ppm/C.

Best regards,

Jim