This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIT4096IPWR

Other Parts Discussed in Thread: OPA355, OPA343, LM2611, DIT4096

OPA355NA
OPA355NA/3K
OPA355NA/250
DIT4096IPWR
OPA343NA
OPA343NA/3K
OPA343NA/250

Hi,

I need ESD information for mentioned parts. Kindly provide us data.

1)Human Body Model, HBM
2)Machine Model, MM

3)Charged Device Model, CDM
LM2611AMF/NOPB
  • Hello Amruta,

    I can help you with the OPA355 and OPA343 op amps. Note that the HBM and MM numbers are the same for the various suffixes you listed:

    OPA343      HBM    500 V       MM     100 V

    OPA355      HBM     4 kV        MM      500 V

    The DIT4096 is a digital audio transmitter and we do not have ESD information about it here in Precision Amplifiers. Please inquire about its HBM/MM ESD peformance on the Audio Converters E2E forum. Also, the LM2611 is a DC-DC converter and not covered on this forum. Contact the Non-isolated DC/DC E2E forum for help with its CDM ESD performance.

    Regards, Thomas

    Precision Amplifiers Applications Engineering

  • Hi Thomas,

    Thanks for your quick response and guidance about remaining parts.