This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer was use OPA2380 and looking for better noise performance.
Now they use OPA2320 to do testing, and set it up as differential amplifier, gain is 33. The input signal is 50mV sin wave.
When the frequency of sin wave increased to 30Khz and it is getting distortion.
Following is the out put signal when the input at 80Khz.
Please help to advice if you have better suggestion for this application.
Hi Anna,
what do we see in the scope plot? Input and output signal?
Can you show us a schematic of your test circuit? Where exactly do you measure?
Kai
Hi Kai,
thanks for your reply
The input signals are two sine signals with 90 degree phase difference. The amplitude of the sine signals is 50 mVpp ,the frequency is 80kHz and the dc offset 0V.
The yellow and blue line are the output signal measured from test circuit which is shown below.
where the offset voltage is 1.5V and signal source is the sine that i mentioned at the beginning part.
Hello Anna,
I have a couple of questions regarding the circuit provided.
Best regards,
Errol Leon
Texas Instruments
Precision Amplifier Applications