Hi,
I want to measure the current across voltage rails which are mentioned below.
Rail 1: 1V @ Max:2.5A
Rail 2: 1.2V @ Max:1A
Rail 3: 1.8V @ Max:0.9A
Rail 4: 3.3V @ Max:0.05A
So I am using 1-4milli ohm resistor(1206 package) for measuring current because of less drop.
So please suggest current sensing IC part number which can sense minimum of 1mA or less and maximum current ratings as mentioned. It will be better if the IC should have integrated ADC with high resolution and more number of channel if possible.
Thanks in Advance.
Regards,
Sathyasai