Part Number: INA226EVM
Other Parts Discussed in Thread: INA226,
Hi,
The configured detection time is 1.1 ms. The length of the inspection line is 300mm x 2.
1. Shunt resistance is 0.000375 ohm.
2. Multimeter is fluke's high-precision multimeter, in the ammeter is fluke clamp ammeter
How to adjust can improve the detection accuracy?
| INA226 Voltage (mV) | high-precision multimeter (mV) |
Voltage error | INA226 current (A) |
Ammeter (A) |
Charger number (A) |
|
| 充电 | -3.738 | -3.816 | -0.078 | 9.96 | 9.9 | 10.01 |
| -18.22 | -18.58 | -0.36 | 48.58 | 49.7 | 50.02 | |
| -36.57 | -37.262 | -0.692 | 97.55 | 99.8 | 99.99 | |
| -55.44 | -56.26 | -0.82 | 147.9 | 150.3 | 149.98 | |
| -74.44 | -75.53 | -1.09 | 198.6 | 200.6 | 200 | |
| -74.67 | -75.62 | -0.95 | 199 | 200.6 | 200 | |
| 放电 | 3.52 | 3.557 | 0.037 | 9.382 | 9.8 | 9.98 |
| 10.73 | 10.96 | 0.23 | 28.63 | 29.8 | 29.96 | |
| 18 | 18.35 | 0.35 | 47.97 | 49.7 | 49.99 | |
| 25.3 | 25.77 | 0.47 | 67.5 | 69.7 | 70 | |
| 34.48 | 35.07 | 0.59 | 91.96 | 94.6 | 95 |
Thank you.