This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91000: LMP9100

Part Number: LMP91000

Dear Community,     

I am working with the lmp91000 and the sensor O2-M2 of Alphasense.

The settings that I used for the sensor O2-M2 are as follows:

LMP91000_TIA_GAIN_350K | LMP91000_RLOAD_100OHM,
LMP91000_REF_SOURCE_INT | LMP91000_INT_Z_50PCT | LMP91000_BIAS_SIGN_POS | LMP91000_BIAS_0PCT,
LMP91000_FET_SHORT_DISABLED | LMP91000_OP_MODE_AMPEROMETRIC

The next picture show how I connect the LMP91000 and the sensor

My problem is with the Vout, My multimeter don't read any voltage. 

There is something wrong with my connections or my configurations?