Part Number: OPA140
Dear Team,
We are learning from the precision lab video.
If we use (+-5V) on OPA140 as the supply voltage.
Function generator to 50kHz, 9Vpp, oV offset, 50% symmetry.
We can see distortion at around 2.0V+.
But when operate in 1kHz the distortion didn't occur(actually a small distortion).
The training material mention OPA140 is actually rail to rail at low frequencies, but how can I find it on the datasheet?
How low the frequency should it be?
Please kindly provide the information
Best regards
Kevin