Part Number: INA381
Hi
1.
Please tell us how to estimate gain error considering temperature drift.
For example, Gain error is offered as 1% as maximum.
Is this value maximum over all opertational temperature range?
Should we consider temperture drift of gain error in addioton even if the maximum 1% gain error is already considered?
2.
Regarding to maximum current consumption with itself, it is 450uA as maximum over operatinal temperature. Is it correct?
3.
When we use multiple devices in same use, is it be possible to connect CMPREF each other at same reference point?
BestRegards