Hi Team,
Could you helpe check if my offset calculation is correct? The op amp I use is opa2196.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Could you helpe check if my offset calculation is correct? The op amp I use is opa2196.
Hello Even,
The output referred voltage offset (Voso) will be primarily due to the amplified input voltage offset (Vosi) mulitplied by the noise gain of the circuit. Vosi is modeled as a voltage source in series with the non-inverting input. For this circuit the noise gain is:
Av = 1 + [R352 / (R354 || R356)] = 1 + [ 180 k / (187 || 187)] = 1926 V/V
Therefore, Vosi will be multiplied by this gain and will appear in the total Voso.
There will also be an offset contribution to Voso due to the input bias current flowing through the various input and feedback resistors.This input bias current related offset will either add to, or subtract from, the offset contibuted by the input voltage offset.
I suggest that you have a look at the TI Precision Labs session, Section 2, that covers the subject of Input Offset Voltage and Input Bias Current. That will provide insight into what makes up the total voltage offset:

Regards, Thomas
Precision Amplifiers Applications Engineering