Part Number: LMV841
Other Parts Discussed in Thread: LMV844, OPA2171, , LMV842, TINA-TI, OPA4171
For OPA2171 you don't only provide a figure for max allowed C_LOAD and recommend R_ISO, you also provide a graph of R_ISO vs C_LOAD for phase margins of 45 and 60 degrees. Is this graph available also for the LMV841/LMV842/LMV844?
I always have at least 1k (2%) "R_ISO" and after that a capacitor of max 33nF (possibly 47nF). Sounds to me like low risk.
I could try to produce the amplitude graph myself, by looking at OPA2171 fig 42, however that would not give me the phase data, and there also are some discrepancies in OPA2171 fig 42 which makes me feel I'm on my own with no reliable help from the datasheet: I thought fig 42 is the open loop gain to which influence of C_LOAD is added, but why is peak gain then 120dB and flat until 100Hz when the open-loop gain in fig 19 says 130dB up to about 3Hz and at 100Hz only 90dB?
(AN-1708 title sounds promising but contains no added value.)