Part Number: INA302
Customer is exploring the options available in INA302. They are planning to use the IC for over current and undercurrent detection. They have 50 units to be tested at a time and have the current ranging from 1A to 30A to be measured. He was doing the calculation and came across the Rsense selection section. Can he uses one Rsense for all the varying current limit?
He observed a mistake in table 2 of the data sheet the VOS_ERROR_MAX shown is 0.48% which he believes is wrong . He gets 0.98% when he recreates the calculation. This also leads to confusion whether to choose same part or not.. But primarily he wants to know whether they can implement 1A to 30A measurement in one IC using DAC methodology. Thank you