Part Number: THS4522
Other Parts Discussed in Thread: ADS8354, TINA-TI
I am using a THS4522 to amplify the signals coming from two full wheatstone bridges. The signals go through the THS4522 and then are converted from analog to digital using the ADS8354 chip. Is there a way to remove the initial offset voltage when no strain is applied? I am currently doing it in the code, after the signal is converted, but the offset does not let me use the entire's converter range to measure the change in strain applied.
Can the THS4522 be controlled to adjust the initial offset to zero? I do not want to use potentiometers, as I am planning on making several of these and they will all have different offset values.