Part Number: OPA209
Hi Sirs,
Sorry to bother you.
OPA209 have some THD+N error
Description:
In the [QC Test Item_11] AI Dynamic test, when imputing the signal of 20KHz / 6.3Vrms(17.825Vpp), the THD shows that there are some abnormal phenomena of Channel AI which is more than -78dB.
This problem can be solved by changing relative OPA209(U10/U15/U20/U25).
We use APx515AI to measure the THD signal of OPA209 directly to avoid the impact of other trace, measuring point as shown in Figure 1.
Measuring 3 pcs of defective OPA209 discovered that the output signal THD of OPA209 is less than 78dB when imputing signal of 20KHz. The difference between the normal OPA209 THD is more than 10dB, as shown in Figure 2, Figure 3.
Actually we have do A-B-A swap analysis, looks this phenomenon is follow IC. The fail rate around 18% (9/50)
We think THD is a typical specification in the TI datasheet and FA is not able to determine a physical cause.
So, could you help us to check this??
Any suggest is welcome, thanks!!