Part Number: LM358
Other Parts Discussed in Thread: RC4558, OPA1678, TLV2170
Hi,
The input (EXC_C) is a sine (0.7V to 4.3V, 2.5V is the middle point),the output (EXC) should be a sine (3.45V to 12.39V, 7.92V is the middle point). But the output had a bit of distortion actually.
Channel 1(yellow) is EXC, channel 2 (green) is the base of 3904. The output of LM358 at PIN1 is the same with EXC. The negative feedback doesn't work. I don't know what happened with this circuit.
channel1 is EXC, channel 2 is EXC_C.
channel 1 is EXC, channel 2 is the input of LM358 at PIN2.