This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2262: What is the closest SINGLE op amp match to the TLC2262/4?

Part Number: TLC2262
Other Parts Discussed in Thread: OPA196, TLC2274, TLC2272, TLC2264, TLV2371

Hello,

I use a lot of TLC2262/4 in my designs.  I find myself needing a SINGLE op amp but there doesn't seem to be one in that family.  Is there another single package op amp at TI with very similar specs?  I need it to operate at 10V single supply and I'd like the low power, low offset, rail to rail output of the TLC2262/4 series.

Thanks!

  • Hi Brian,

    Note that I edited this post because I made reference to the TLC2272/TLC2274 which was incorrect. However, the OPA196 would serve as a good single op amp replacement for the TLC2262.

    You are probably going to get a couple of suggestions!

    The TLC2262/TLC2264 is a little older amplifier and you can now get similar performance from a single, with much lower operating current. I suggest taking a look at the OPA196. It is a newer product that was released just last year:

    http://www.ti.com/lit/ds/symlink/opa196.pdf

    The electrical performances meet or exceed that of the TLC2262/TLC2264 for most parameters.

    The OPA196 features rail-to-rail input and output, and is offered in a variety of different package types.

    Regards, Thomas

    Precision Amplifiers Applications Engineering

  • Hi Brian,

    Thomas gave you a good suggestion, I'll add another - the TLV2371 is worth a look as well. A little higher offset voltage but similar specs otherwise.

    -Paul