Part Number: ISO121
Other Parts Discussed in Thread: AMC1300, AMC1301
Hi,
My applicaiton is to measure a current-source (200nA to 10uA) of 50ohm, and the Isolation is to be 3KV and above. I have selected ISO121 as an Isolation Amplifier for the rated 5KVdc barrier.
My Questions:
1. ISO121 requires +-15V, and as the barrier is above 3KV, I have to use a DC/DC converter, which is very noisy. Can ISO121 supports single Power-Supply of +15V, and I can do away with the +-15V? I am currently using a DC/DC converter and the noise is about 40mV. As my input signal is small, I need the noise to be lower for good SN ratio.
2. The recommended Gain Adjust in Data-sheet, is an input of 1Kohm(R1), can this resistance be changed to 100kohm? Should the sense resistance be changed to 200kohm for a gain of 5?
Thanks